Technical Information on the AS-i Gateway

 

Environmental profile of the AS-i Gateway

The electrical and/or environmental characteristics of the AS-i Gateway may deviate from the characteristics of the Schneider Electric safety-related modules as it relates to your control system. Therefore, validate that the AS-i Gateway is integrated into environments that are suitable and therefore compatible with the Schneider Electric system.

Refer to the corresponding documentation or specification provided by Bihl+Wiedemann with the AS-i Gateway.

WARNING

INOPERABLE EQUIPMENT

Verify that all of the electrical and environmental characteristics of the equipment meet the operating conditions and requirements of the embedded safety system.

Failure to follow these instructions can result in death, serious injury, or equipment damage.

Features & Facts

Further Information

For a detailed description of the AS-i Gateway, its interfaces, and connectivity, refer to the product sheets and user manuals provided by the AS-i Gateway manufacturer Bihl+Wiede­mann.

System limits for AS-i Gateway in PacDrive 3 systems: when inte­grated into the Schneider Electric PacDrive 3 Safety System, the func­tional range of the AS-i Gateway is available with no restrictions.

Hardware: interfaces/connectivity of the AS-i/Sercos III Safety Gateway BWU 2984

ASi_Gateway.png

(1)

Chip card for storing the AS-i master configuration (control functionality, configured in ASIMON)

(2)

Diagnostic interface for connecting the PC running ASIMON or a Safe Link connection to a further AS-i Gateway (cross-communication)

(3)

LEDs for status indication

(4)

Field bus interface for connecting the Sercos field bus

(5)

LC display for status indication

(6)

Buttons for manual operation

(7)

+ASI1-: AS-i circuit 1 for connecting a maximum of 31 safety-related or 62 standard (non-safety-related) slaves

(8)

+ASI2-: AS-i circuit 2 for connecting a maximum of 31 safety-related or 62 standard (non-safety-related) slaves

(9)

ASI+PWR-: supply voltage for the AS-i circuits

NOTE:

Electrical installation and start-up of AS-i Gateway devices is not part of this integration guide. Refer to the appropriate documentation provided by Bihl+Wiedemann.